990–5809D-001

Connect the Emergency Power Off (EPO)

Do not connect any circuit to the EPO terminal block unless it can be confirmed that the circuit is Class 2/SELV.

All circuits connected must have the same 0 V reference.

  1. Open the door to ensure that the cables will not be too tight.
  2. Route the cables from your EPO through the top or bottom of the I/O cabinet and to the EPO terminals J4936–J4938 on 0P647 as shown in Prepare the I/O Cabinet for Signal Cables in Top Cable Entry Systems and Prepare the I/O Cabinet for Signal Cables in Bottom Cable Entry Systems.
  3. Connect the building EPO according to one of the options below.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.