990–5809D-001

Install Busbars between the Power Cabinets

  1. Install the grounding busbars 880-99027 from the installation kit 0H-9162, or 0H-9102* between all power cabinets.

    Front View of Two Power Cabinets

  2. Install the interconnection busbars from the installation kit 0H-9162, or 0H-9102* between all power cabinets.
    1. Install the three input interconnection busbars 0M-97885.

      Front View of the Busbar Connections

    2. Install the battery – interconnection busbar 0M-819336.
    3. Install the battery + interconnection busbar 0M-140035.

      Front View of Busbar Connections

    4. Install the output interconnection busbars 0M-97886.
    5. Install the neutral interconnection busbar 880-10146 or 880-9720*.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.