990–5809D-001

Connect the Signal Cables between the I/O Cabinet and the Classic Battery Cabinets

NOTE: The illustration below shows a system with four battery banks each consisting of one classic battery cabinet. Connect signal cables according to the number of classic battery cabinets in your installation.
NOTE: If you have two classic battery cabinets in your battery bank, see Connect the Signal Cables between Two Classic Battery Cabinets in One Battery Bank for information on how to connect signal cables between two classic battery cabinets in one battery bank.
  1. Route the signal cables from the battery banks through the top or bottom of the I/O cabinet to the boards.
  2. Connect the signal cables between the I/O cabinet and the classic battery cabinets.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.