990–5809D-001

Remove the Power Cabinet from the Pallet

NOTICE
RISK of equipment damage
Ensure that the floor is level and can support the weight of the jack when it carries the cabinet.
Failure to follow these instructions can result in equipment damage.
NOTICE
RISK of equipment damage
Be careful not to damage the cabinets when using the jack.
Failure to follow these instructions can result in equipment damage.
  1. Take the installation kit 0M-816661 shipped with the I/O cabinet. Use the jack and the floor protection plate in the kit for all cabinets in this procedure.
  2. Place the floor protection plate under the pallet on the rear of the cabinet.

    Rear View of the Power Cabinet

  3. Place the jack from the installation kit in the hole in the transport bracket on the rear of the cabinet.
    WARNING
    hazard of Tilting
    Do not use a jack in the front and rear transport bracket at the same time.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  4. Loosen and remove the bolts from the rear transport bracket and from the middle pallet part. Save the two middle pallet parts for step 8.

    Rear View of the Power Cabinet

  5. Use a drilling machine with the provided hexagonal socket to activate the jack, slide it into position in the bracket, and to make contact with the floor protection plate.
    NOTE: Reduce the drill torque to minimum to prevent kickback.
  6. Use the jack to lift the pallet to the top position.
  7. Remove the rear and middle pallet parts. Save the middle pallet part for step 8.
    WARNING
    hazard of serious injury
    Do not put your hands or feet under the cabinet while removing the pallet parts.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.

    Rear View of the Power Cabinet

  8. Place the pallet parts from step 4 and 7 under the transportation bracket.

    Rear View of the Power Cabinet

  9. Use a drilling machine to lower the cabinet down onto the support.
  10. Move the floor protection plate and the jack from the rear to the front side.

    Rear View of the Power Cabinet

  11. Loosen and remove the bolts from the front transport bracket.

    Front View of the Power Cabinet

  12. Use a drilling machine with the provided hexagonal socket to activate the jack, slide it into position in the bracket, and to lift the pallet to the top position.
  13. Remove the front pallet parts.
    WARNING
    hazard of serious injury
    Do not put your hands or feet under the cabinet while removing the wooden plate.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.

    Front View of the Power Cabinet

  14. Use the jack to lower the cabinet onto the floor until the wheels connect with the floor. Remove the jack and the floor protection plate.
  15. Wheel the cabinet away and remove the remaining pallet parts.
    WARNING
    Hazard of tilting
    Be alert to uneven floors and doorsteps when moving the cabinet on its wheels to avoid overbalancing and tipping the cabinet.

    Front View of the Power Cabinet

  16. Remove the front and rear transportation brackets.
    The cabinet can now be moved on the built-in wheels to the installation area.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.