990–5809D-001

Connect the Signal Cables between Two Classic Battery Cabinets in One Battery Bank

NOTE: The procedure is identical for all battery banks with two classic battery cabinets.
  1. Remove the jumper between J3802 pin 3 and 4 in classic battery cabinet A.
  2. Connect the signal cables between classic battery cabinet A and classic battery cabinet B.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.