990–5809D-001

Overview of Configurations

Breakers in the System

UIB Unit input breaker
SSIB Static switch input breaker
BB Battery breaker
MBB Maintenance bypass breaker
UOB Unit output breaker
BF2 Backfeed protection switch

Overview of UPSs with 1000 kW I/O Cabinet – Single Utility/Mains System

The illustration shows a 750 kW UPS. The principle is the same for the other UPSs with the 1000 kW I/O cabinet.

Galaxy VX 750 kW UPS

Overview of UPSs with 1000 kW I/O Cabinet – Dual Utility/Mains System

The illustration shows a 750 kW UPS. The principle is the same for the other UPSs with the 1000 kW I/O cabinet.

Galaxy VX 750 kW UPS

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.