990–5809D-001

Recommended Upstream Protection and Cable Sizes

DANGER
hazard of electric shock, explosion, or arc flash
A readily accessible breaker is required for upstream protection. Maximum fault current disconnection time: 46 seconds at 200% input.
Failure to follow these instructions will result in death or serious injury.
NOTE: Overcurrent protection is to be provided by others.

Cable sizes in this manual are based on table B.52.12 and B.52.13 of IEC 60364–5–52 with the following assertions:

  • 90 °C conductors

  • An ambient temperature of 30 °C

  • Use of copper or aluminium conductors

  • Installation method F4 for DC cables and installation method F5 for AC cables, corrected for single layer in perforated cable tray.

PE cables are sized in accordance with IEC 60364-5-54 table 54.2 Minimum cross-sectional area of protective conductors.

NOTE: Alwasy consider the PE size according to the complete electrical installation.

If the ambient temperature is greater than 30 °C, larger conductors are to be selected in accordance with the correction factors of the IEC.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.