990–5809D-001

Overview of Supplied Installation Kits

Installation Kits Shipped with the I/O Cabinet

Installation Kit 0M-92449

Part Used in Number of Units
Display
0N-96367
Do not install. Installation must be performed by Schneider Electric.

1

M4x10 torx screw with washer

4

Installation Kits Shipped with the Power Cabinet

Installation Kit 0H-9162 or 0H-9102

NOTE: These installation kit parts are shipped in the packaging of the power cabinet.
Part Used in Number of Units
Rear anchoring bracket for power cabinet 0M-818242 Mount the Rear Anchoring Brackets

1

M8x20 hexagonal torx with washer
803–8590

2

Front anchoring bracket for power cabinet 0M-816684 Mount the Front Anchoring Bracket

1

Long top baying bracket 0M-821220 Position the Cabinets

1

M6x16 torx screw with washer
803–0686

15

1 mm leveling shims
870–2538

10

Ground interconnection busbar 880–5259 or 880–99027* from power cabinet to power cabinet Install Busbars between the I/O Cabinet and the Power Cabinet and Install Busbars between the Power Cabinets

1

M8x35 mm hexagonal torx with washer
803–8588

4

M8 nut with washer
803–8007

4

Interconnection busbar 880-10146 or 880–9720* from power cabinet to power cabinet (neutral)

1

Interconnection busbar 0M-140035 power cabinet to power cabinet (battery +)

1

Interconnection busbar 0M-97886 power cabinet to power cabinet (output)

3

Interconnection busbar 0M-819336 power cabinet to power cabinet (battery -)

1

Interconnection busbar 0M-97885 power cabinet to power cabinet (input)

3

M10 nut with washer
803–1005

24

M10x35 hexagonal torx with washer
803–8587

12

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.