990–5809D-001

Position the Cabinets

DANGER
hazard of electric shock, explosion, or arc flash
Do not step/walk on top of the cabinets.
Failure to follow these instructions will result in death or serious injury.
NOTE: For some of the steps below, only the power cabinet is shown. The procedure is the same for all cabinets.
  1. Install the interconnection cover from the installation kit 0M-99582 on the right side (front view) of the right-most power cabinet and fasten with the M6 nuts.

    Front View of the Power Cabinet

  2. Move the side panel from the right side (front view) of the I/O cabinet and install it on the right side of the right-most power cabinet.
  3. Perform the following steps on all power cabinets:
    1. Remove the 12 screws and open the fan door of the power cabinets.
    2. Disconnect the cable between the fan door and the power cabinet.
    3. Lift the fan door up and remove it.
    4. Disconnect the two cables from each of the two middle power blocks.
    5. Loosen the screws and pull out the middle power blocks. Be careful not to damage the cables.
      NOTICE
      risk of equipment damage
      Cover the power blocks when removed from the power cabinet to avoid dust in the power blocks.
      Failure to follow these instructions can result in equipment damage.
    6. Loosen the screws and remove the plate below the power blocks.

      Top Front View of the Power Cabinet

  4. Install the fan doors temporarily on all power cabinets and fasten with two screws.
    NOTICE
    risk of equipment damage
    The fan doors must be installed to avoid damaging the signal cables when pushing the power cabinets into position.
    Failure to follow these instructions can result in equipment damage.
  5. Push the I/O cabinet and the power cabinets one by one into position against the rear anchoring brackets – the cabinets will connect to the conic outcroppings on the brackets.
  6. Fasten the cabinets to the rear anchoring brackets by tightening the bolts on the front of the cabinet. Torque to 50 Nm (36.87 lb-ft).
  7. Remove the fan doors of the power cabinets.
  8. Lower the two front feet on all cabinets until they connect with the floor – use a bubble-leveler to ensure that the cabinets are level. Use the provided levelling shims if necessary.
  9. Install the top baying bracket on the top of the cabinets and fasten with the provided screws.

    I/O Cabinet and Two Power Cabinets

  10. Mount the M6 screws from the installation kit from right to left in the five marked positions between the power cabinets and in the four marked positions between the power cabinet and the I/O cabinet to tighten the cabinets together.

    From Power to Power Cabinet

    From Power to I/O Cabinet

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.