990-5452N-001

Access Password-Protected Screens

NOTE: The default administrator username/password are admin/admin. Change the password after logging in the first time, and change the password regularly.
NOTE: The default user username/password are config/config.
  1. When prompted for the password, tap the Username field to access the keyboard.
  2. Tap the username field, type in your username, and tap Enter.
  3. Tap the Password field, type in your password, and tap Enter.
  4. Tap Login.
  5. Tap Close or the X button to exit the Login pop-up screen.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?