990-5452N-001

Transfer the Parallel System from Requested Static Bypass to Normal Operation

Please note that only the administrator can change operation mode.
  1. From the home screen on the display select Control.
  2. Tap the Transfer to Inverter Operation button.
    NOTE: If the conditions for performing the transfer are not met, the button will be grayed out.
  3. Verify that the System Operation Mode changes to Inverter.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?