990-5452N-001

Perform an Annunciators Test

  1. From the home screen on the display select Tests > Annunciators.
  2. Tap the Start button to initiate the test.

    During the annunciators test the LEDs on the display and the mimic diagram and the audible alarm are tested.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?