990-5452N-001

Set the UPS Identification

NOTE: User Defined Name and User Defined Location must be configured via the network management interface. For more information see Access a Configured Network Management Interface.
  1. From the home screen on the display select Configuration > UPS > Identification.
  2. Select to have the UPS identified via Model Name, User Defined Name or User Defined Location.
  3. Tap arrow to the right to go to the next configuration screen.
  4. Tap the text box and type a name for the individual disconnect devices or keep the default settings. The alias is limited to four characters.
  5. Tap OK to confirm your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?