990-5452N-001

View the Active Alarms

When there is an active alarm in the system, a symbol indicating the alarm level is shown in the top right corner of the screen and the buzzer is active.

  1. From the home screen on the display select Status > Active Alarms. Tapping the display will also silence the buzzer temporarily without login. By logging in and tapping the display, the buzzer will be silenced permanently.
  2. You can now browse through the list of active alarms using the left and right arrows.
  3. Tap the Refresh button to update the list with the latest active alarms.

Alarm Levels

There are three alarm levels:

  • Critical: Take immediate action and call Schneider Electric.

  • Warning: The load remains supported, but action must be taken. Call Schneider Electric.

  • Informational: No immediate action required. Check the cause of the alarm as soon as possible.

Alarm Messages

Alarm/ Event Severity

Display text

Description Corrective action
Alarm Warning Abnormal state at input contact zone A An abnormal state exists for integrated Environmental Monitor input contact zone A. Please check the environment.
Alarm Warning Abnormal state at input contact zone B An abnormal state exists for integrated Environmental Monitor input contact zone B. Please check the environment.
Alarm Warning

Air Filter technical check recommended

The air filters need to be checked as preventive maintenance is recommended.

The air filters may need to be replaced.
Alarm Warning

Ambient temperature high

Ambient temperature is high.

 
Alarm Warning

Ambient temperature out of tolerance

The ambient temperature out of tolerance.

 
Alarm Warning

Batteries are discharging

The load is drawing more power than the UPS can draw from the input, causing the UPS to draw power from the batteries.

 
Alarm Warning

Battery breaker BB1 open

Battery breaker BB1 is open.

 
Alarm Warning

Battery breaker BB2 open

Battery breaker BB2 is open.

 
Alarm Warning

Battery breaker BB3 open

Battery breaker BB3 open.

 
Alarm Warning

Battery breaker BB4 open

Battery breaker BB4 open.

 
Alarm Warning Battery capacity is below minimum acceptable level The battery capacity is below the minimum acceptable value according to UPS power rating. Risk of battery damage. Change battery configuration and/or add larger capacity battery.
Event Informational

Battery breakers tripped

To prevent the batteries deep discharging, the battery breakers have been tripped by the system.

Close the battery breakers manually.
Alarm Warning

Battery condition is poor

Battery capacity is lower than 50%.

Batteries should be replaced.
Alarm Warning

Battery condition is weak

Battery capacity is between 50% to 75%.

 
Alarm Warning

Battery is below minimum acceptable runtime

The battery runtime is below configured minimum acceptable value.

 
Alarm Critical

Battery is not working correctly

A battery is not working correctly.

Please contact Schneider Electric.
Alarm Warning

Battery room ventilation inoperable

Input relay indicates that the battery room ventilation is not working correctly.

 
Alarm Warning

Bypass backfeed breaker (BF2) open

Bypass backfeed breaker (BF2) is open, and the UPS is prevented from running in normal operation.

 
Alarm Warning

Breaker MBB closed

Maintenance bypass breaker MBB is closed, feeding the load with unprotected power from bypass.

 
Alarm Warning

Breaker SIB open

System isolation breaker SIB is open, and system cannot feed the load.

 
Alarm Warning

Breaker SSIB open

Bypass static switch input breaker SSIB is open, making static bypass operation unavailable.

 
Alarm Warning

Breaker UIB open

Unit input breaker UIB is open, and the UPS is prevented from running in normal operation.

 
Alarm Warning

Breaker UOB open

Unit output breaker UOB is open, and UPS cannot feed the load.

 
Alarm Warning

Bypass frequency out of tolerance

Bypass input frequency is out of tolerance.

Check bypass input frequency and bypass input frequency setting.
Alarm Warning

Bypass phase missing

Bypass input is missing a phase.

Check bypass input. Please contact Schneider Electric.
Alarm Warning

Bypass phase sequence incorrect

The phase rotation on bypass input is incorrect.

Check bypass input. Please contact Schneider Electric.
Alarm Warning

Bypass voltage out of tolerance

Bypass input voltage is out of tolerance and UPS is prevented from going into requested bypass mode.

 
Alarm Warning

Charge power is reduced

The battery charge power has been reduced.

The input for this functionality was activated, or the input current has reached the maximum limit. Please contact Schneider Electric.
Alarm Warning

Communication cable termination missing or damaged

One or more communication cable terminators is/are missing or damaged.

 
Alarm Warning Confirm redundancy lost and/or transfer to Forced Static Bypass Off button has been pushed and user must confirm that the redundancy will be lost and/or system will transfer to Forced Static Bypass.  
Alarm Warning

Confirm Turn Load Off

Off button has been pushed while inverter is on and with no bypass available. User must confirm that the UPS turns off the power to the load.

Confirm turn off either via display or by pushing the off button again.
Alarm Informational

Customer Input 1 activated

Customer input relay 1 is activated.

 
Alarm Informational

Customer Input 2 activated

Customer input relay 2 is activated.

 
Alarm Warning

Delayed transfer from battery to normal operation

The delayed transfer from battery to normal operation is active.

 
Alarm Warning

Display communication is lost

Main Controller is unable to communicate with the display.

Please contact Schneider Electric.
Alarm Warning

Display firmware incompatibility detected

The firmware of the display is detected as incompatible with the rest of the system.

Perform a firmware update.
Alarm Critical

EPO Switch Activated

An emergency power off (EPO) switch is activated.

Deactivate the Emergency Power Off (EPO) switch.
Alarm Warning

External battery monitoring detected fault

Input relay indicates external battery monitoring detected fault

 
Alarm Critical

External charger off command: activated

Input relay for charger off is activated.

Please contact Schneider Electric.
Alarm Critical

External energy storage monitoring: major alarm

Input relay indicates external energy storage monitoring has detected a major alarm.

Please contact Schneider Electric.
Alarm Warning

External energy storage monitoring: minor alarm

Input relay indicates external energy storage monitoring has detected a minor alarm

Please contact Schneider Electric.
Alarm Warning

External sync frequency out of tolerance

External sync frequency is out of tolerance.

Check external sync frequency.
Alarm Warning

External sync phase missing

External sync is missing a phase.

Check external sync.
Alarm Warning

External sync phase sequence incorrect

The phase rotation on external sync is incorrect.

Please contact Schneider Electric.
Alarm Warning External sync temporarily disabled External sync has been temporarily disabled because UPS cannot lock and syncronize to the external sync source. Check external sync.
Alarm Warning

External sync voltage out of tolerance

External sync voltage is out of tolerance and UPS is prevented from going into external sync mode.

 
Alarm Warning

Fan inoperable

UPS has one or more inoperable fans. Fan redundancy is lost.

 
Alarm Critical

Firmware update - Incorrect UPS operation mode

The UPS is no longer in the correct operation mode during firmware update. Risk of load drop.

Transfer UPS to maintenance bypass.
Alarm Warning Firmware versions in parallel UPS units are not identical The firmware versions in parallel UPS units are not identical. Firmware update all UPS units in the parallel system to the same version.
Alarm Critical Flywheel inoperable Input relay indicates that the flywheel is not working correctly.  
Alarm Informational

Forced battery operation activated

Forced battery operation has been activated by user.

 
Alarm Critical

General parallel system event

The parallel system is not configured correctly or is not working correctly.

Please contact Schneider Electric.
Alarm Informational

Genset is supplying the UPS

Input relay indicates that a genset is supplying the UPS.  
Alarm Warning

Ground fault detected

Input relay indicates that a ground fault has been detected.

Please contact Schneider Electric.
Alarm Warning

High Battery Temperature Level

The battery temperature is above the Alarm setting.

Check the battery temperature. A high temperature may decrease the battery lifetime.
Alarm Informational

High Efficiency Mode disabled

High efficiency mode is disabled from an input relay.

 
Alarm Informational

High efficiency mode has been disabled by the system

High Efficiency Mode is disabled by the system as the maximum number of transitions has been exceeded.

Enable high efficiency mode again, or disable it permanently.
Alarm Informational

High efficiency mode is disabled due to bypass UTHD is above configured limit

High efficiency mode is disabled due to bypass UTHD is above configured limit.

 
Alarm Warning

High humidity threshold violation at remote sensor

A high humidity threshold violation exists for integrated Environmental Monitor sensor.

Please check the environment.
Alarm Warning

High temperature threshold violation at remote sensor

A high temperature threshold violation exists for integrated Environmental Monitor sensor.

Please check the environment.
Alarm Warning

Incorrect UPS configuration detected

Incorrect UPS configuration detected.

 
Alarm Warning

Input frequency out of tolerance

Mains input frequency is out of tolerance.

Check input frequency and input frequency setting.
Alarm Warning

Input phase missing

Input is missing a phase.

Check input. Please contact Schneider Electric.
Alarm Warning

Input phase sequence incorrect

The phase rotation on input is incorrect.

Check input. Please contact Schneider Electric.
Alarm Warning

Input voltage out of tolerance

Mains input voltage is out of tolerance.

 
Alarm Warning

Inverter is Off due to a request by the user

The inverter is off due to a request by the user.

 
Alarm Warning

Inverter output is not in phase with bypass input

The UPS inverter output is not in phase with the bypass input.

 
Alarm Warning

Li-Ion AC Supply Breaker BMS:B1/BMS:B2 open

One or both Li-Ion BMS AC Supply Breakers are open.

 
Alarm Warning

Lost communication to remote sensor

Lost the local network management interface-to-integrated Environmental Monitor.

Please check the environment.
Alarm Warning

Lost parallel redundancy

The load exceeds limit for an N+x UPS in redundancy (x is the configurable parallel redundancy).

Reduce the load on the system.
Alarm Warning

Low Battery Temperature Level

The battery temperature is below the Alarm setting.

 
Alarm Warning

Low humidity threshold violation at remote sensor

A low humidity threshold violation exists for integrated Environmental Monitor sensor.

Please check the environment.
Alarm Warning

Low temperature threshold violation at remote sensor

A low temperature threshold violation exists for integrated Environmental Monitor sensor.

Please check the environment.
Alarm Warning

Magelis 10 inch display firmware incompatibility detected

The firmware of the Magelis 10 inch display is detected as incompatible with the rest of the system.

Perform a firmware update.
Alarm Warning

Maintenance bypass breaker (MBB) closed

Maintenance bypass breaker (MBB) is closed, feeding the load with unprotected power from bypass.

 
Alarm Warning

Maximum humidity threshold violation at remote sensor

A maximum humidity threshold violation exists for integrated Environmental Monitor sensor.

Please check the environment.
Alarm Warning

Maximum temperature threshold violation at remote sensor

A maximum temperature threshold violation exists for integrated Environmental Monitor sensor.

Please check the environment.
Alarm Informational

Mega Tie is activated

Dry contact input indicates that Mega Tie is activated.

 
Alarm Warning

Minimum humidity threshold violation at remote sensor

A minimum humidity threshold violation exists for integrated Environmental Monitor sensor.

Please check the environment.
Alarm Warning

Minimum temperature threshold violation at remote sensor

A minimum temperature threshold violation exists for integrated Environmental Monitor sensor.

Please check the environment.
Alarm Warning

Modular battery breaker open

Modular battery breaker is open.

 
Alarm Warning

Modular battery cabinet is not working correctly

Modular battery cabinet is not working correctly.

Check battery cabinet. Please contact Schneider Electric.
Alarm Warning

NMC 1 firmware incompatibility detected

The firmware of the NMC in Smart Slot 1 is detected as incompatible with the rest of the system.

Perform a firmware update.
Alarm Warning

NMC 2 firmware incompatibility detected

The firmware of the NMC in Smart Slot 2 is detected as incompatible with the rest of the system.

Perform a firmware update.
Alarm Warning

Not enough UPS units ready to turn on inverter

One or more parallel UPS units have been requested to turn on inverter, but not enough UPS units are ready for system to enter inverter on operation.

Turn on inverter of more UPS units and/or check the setting Minimum Number of UPS Required to Supply Load.
Alarm Warning

Output frequency out of tolerance

Output frequency is out of tolerance.

Check output frequency and output frequency setting.
Alarm Warning

Output voltage out of tolerance

The output voltage is out of tolerance.

 
Alarm Warning

Overload on installation

The load exceeds 100% of rated installation capacity.

Reduce load on system.
Alarm Warning

Overload on UPS due to high ambient temperature

The load exceeds the rated capacity when running with high ambient temperature.

Reduce load on system or ambient temperature.
Alarm Warning

Overload on UPS present. Load below continuous overload threshold

Reduce load on system or check for output short circuit.

The load exceeds 100% of rated capacity. Load is below the continuous overload threshold.
Alarm Warning Overload or short circuit on UPS Reduce load on system or check for output short circuit. The load exceeds 100% of rated capacity or there is a short circuit on the output.
Alarm Warning

Parallel communication lost on PBUS cable 1

PBUS cable 1 may be damaged.

Replace parallel cable 1 (PBUS1).
Alarm Warning

Parallel communication lost on PBUS cable 2

PBUS cable 2 may be damaged.

Replace parallel cable 2 (PBUS2).
Alarm Warning Parallel mixed operation mode One or more parallel UPS units are operating in battery operation, while others are operating in normal operation.  
Alarm Warning

Parallel unit not present

Main Controller is unable to communicate with parallel UPS X. The UPS might have been powered down or communication cables may be damaged.

 
Alarm Warning

Power cabinet inoperable

Power cabinet is inoperable.

Please contact Schneider Electric.
Alarm Warning

Power cabinet mixed operation mode

One or more power cabinets are operating in battery operation, while others are operating in normal operation.

 
Alarm Warning

Power cabinet redundancy lost

The configured power cabinet redundancy is lost, either because the output load is too high, or because there are not enough power cabinets available.

Reduce the load on the system.
Alarm Critical

Power cabinet surveillance internal event detected

Power Cabinet Surveillance detected an internal event.

Please contact Schneider Electric.
Alarm Warning

Requested Bypass command from input contact activated

Requested Bypass command from input contact activated.

 
Alarm Critical

Restricted air flow

Restricted air flow.

This could be caused by a clogged air filter or other obstacle blocking air flow.
Alarm Warning

RTC backup battery is discharged

The RTC backup battery is discharged or the time is not set correctly.

 
Alarm Critical

Self-test - Did not pass

Self-test did not complete correctly.

Check event log and active alarms for more details.
Alarm Warning

Startup recommended

The product has been running overtime without startup.

Please contact Schneider Electric for secure start-up.
Alarm Critical

Static bypass switch inoperable

Static bypass switch is inoperable. UPS is prevented from going into static bypass operation.

Please contact Schneider Electric.
Alarm Warning

Static bypass switch warning

The static bypass switch needs a technical check but is still fully operational.

Please contact Schneider Electric.
Alarm Critical

Surveillance detected fault

Surveillance detected fault.

Please contact Schneider Electric.
Alarm Warning

Synchronization unavailable - system is freerunning

The UPS is unable to synchronize to the bypass input, external source or parallel system.

 
Alarm Warning

System isolation breaker (SIB) open

System isolation breaker (SIB) is open, and system cannot feed the load.

 
Alarm Critical

System locked in bypass operation

The system is locked in bypass operation.

The system has toggled between inverter operation and bypass operation more than 10 times within 1 minute. Please activate on button to transfer back to normal operation.
Alarm Critical

System operation mode - Forced Static Bypass

The system is in bypass in response to a critical event or an inverter off request.

 
Alarm Warning

System operation mode - Maintenance Bypass

The system load is supplied through Maintenance Bypass Breaker (MBB).

 
Alarm Critical

System operation mode - Off

The system output power is turned off.

 
Alarm Warning

System operation mode - Requested Static Bypass

The system is in bypass in response to the UPS front-panel or a user-initiated software command, typically for maintenance.

 
Alarm Critical

System operation mode - Static Bypass Standby

The system is in static bypass standby operation in response to a critical event or an inverter off request.

 
Alarm Warning

Technical Check recommended

The product and its batteries need to be checked as preventive maintenance is recommended.

Please contact Schneider Electric.
Alarm Warning

Transfer from battery to normal operation delay activated

Input relay indicates that the transfer from battery to normal operation delay is activated.

 
Alarm Warning

Unit input breaker (UIB) open

Unit input breaker (UIB) is open, and the UPS is prevented from running in normal operation

 
Alarm Warning

Unit output breaker (UOB) aux wiring not correct

Unit output breaker (UOB) aux wiring is not correct.

Please check UOB aux wiring. Both circuits must connect to a normally open switch.
Alarm Warning

Unit output breaker (UOB) open

Unit output breaker (UOB) is open, and UPS cannot feed the load.

 
Alarm Warning

UPS locked in static bypass mode is activated

Input relay for UPS locked in static bypass mode is activated.

 
Alarm Critical

UPS configuration incorrect

UPS is configured incorrectly.

Please contact Schneider Electric.
Alarm Warning

UPS operation mode - Battery

On battery power in response to an input power problem.

 
Alarm Informational

UPS operation mode - Battery Test

On battery power in response to a test of the performance of the batteries.

 
Alarm Critical

UPS operation mode - Forced Static Bypass

The UPS is in bypass in response to a critical event or an inverter off request.

 
Alarm Informational

UPS operation mode - Initialize

The UPS is initializing.

 
Alarm Informational

UPS operation mode - Inverter Standby

The UPS is ready to enter battery operation but awaits permission from the system. UPS output is off.

 
Alarm Warning

UPS operation mode - Maintenance Bypass

The UPS load is supplied through Maintenance Bypass Breaker (MBB).

 
Alarm Critical

UPS operation mode - Off

The output power is turned off.

 
Alarm Warning

UPS operation mode - Requested Static Bypass

The UPS is in bypass in response to the UPS front-panel or a user-initiated software command, typically for maintenance.

 
Alarm Warning

UPS operation mode - Static Bypass Standby

The UPS is ready to enter static bypass but awaits permission from the system. UPS output is off.

 
Alarm Critical

UPS settings reset to default

Unit settings has been reset to default. The UPS is locked in off operation until settings are confirmed.

Please contact Schneider Electric.
Alarm Warning

Warranty expiring soon

The product is reaching the end of warranty.

Please contact Schneider Electric.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?