990-5452N-001

Enable Peak Shaving Mode

Peak Shaving Mode allows the UPS to reduce peak power consumed from the utility/mains supply.

NOTE: Peak shaving mode must be enabled locally by Schneider Electric during service configuration to make this selection available, but it must be controlled via a remote software application. Contact Schneider Electric for more details.
  1. From the home screen on the display select Configuration > UPS > Software Defined Power.
  2. For Peak Shaving Mode select Enable.
  3. Tap OK to confirm your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?