990-5452N-001

View the Active Alarms

  1. Tap the symbol in the top right corner of the screen.
  2. You can perform the following operations on the Active Alarms screen:
    1. Tap the arrows to browse through the list of active alarms.

      The active alarms are colored according to the alarm level:

      • Green: No active alarms present

      • Blue: Informational alarm present

      • Yellow: Warning alarm present

      • Red: Critical alarm present

    2. Tap the recycle bin button to clear the active alarms list.*
    3. Tap the Acknowledge button to stop the flashing of the active alarms.
  3. Tap the home button to exit the active alarms list.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?