990-5452N-001

Shut Down System Operating as Frequency Converters

Use this procedure to shut down a single system, a parallel system operating as frequency converters.

NOTE: Only operate a disconnect device when the associated disconnect device LED is green.
  1. From the home screen on the display, select Control > Shutdown Wizard. Select Shutdown ending in Off Operation and follow the steps which appear on the screen.
    NOTE: The following is a generic shutdown procedure. Always follow the steps of the Shutdown Wizard which are specific to your system.
  2. Open UOB.
  3. Open battery disconnect devices (if present).
  4. Open UIB.
  5. Repeat steps 1 to 4 on each Galaxy VX in the parallel system.
  6. Open SIB (if present).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?