990-5452N-001

View the Display Log

NOTE: This log is only related to the display operation and not to the operation of the UPS system.
  1. From the home screen on the display select Logs > Display.
  2. You can perform the following operations in the log:
    1. Tap the arrows to browse through the list of events.
    2. Tap the recycle bin button to clear the log.*
  3. Tap the home button to exit the log.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?