990-5452N-001

Perform a Battery Test

Prerequisites:

  • The batteries must be more than 50% charged.

  • The runtime available must be more than 4 minutes.

  • The operation mode must be normal operation, eConversion, or ECO mode.

  • The system operation mode must be normal, eConversion, or ECO mode.

This feature performs a number of tests on the batteries, such as fuse-blown check, weak battery detection. The test will discharge the battery, and use about 10% of the total capacity. Meaning if you have 10 minutes of runtime, the test will run for 1 minute. The Battery Test can be set up to run automatically in different time intervals (from weekly and up to once a year).

  1. From the home screen on the display select Tests > Battery Test.
  2. Tap the Start Battery Self-Test button.
    NOTE: If you wish to manually stop the battery self-test, tap the Abort Battery Self-Test button.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?