990-5452N-001

Start-Up System Operating as Frequency Converters

Use this procedure to start up a single system, a parallel system working as frequency converters, or to start up a single frequency converter and add it into a running parallel system working as frequency converters.

NOTE: Only operate a disconnect device when the associated disconnect device LED is green.
  1. Close UIB.
    This will power up the display interface after approximately 30 seconds.
  2. From the home screen on the display, select Control > Startup Wizard. Select Startup from Off Operation and follow the steps which appear on the screen.
    NOTE: The following is a generic startup procedure. Always follow the steps of the Startup Wizard which are specific to your system.
  3. Close the battery disconnect devices (if present).
  4. Close UOB.
  5. Close SIB.
  6. Tap Turn Inverter On on the display interface.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?