990-5452N-001

Configure Reminder Settings

When the air filters have been replaced, the reminders settings must be updated.
  1. From the home screen on the display select Configuration > Reminders.
  2. Configure the following settings:
    1. Reminders Signalling: Select Enable to enable the display of all reminders.
    2. Reminder: Select Enable to enable the display of reminders for air filter replacement.
    3. Duration before 1st Reminder: Set the time in weeks before the first reminder is shown.
    4. Elapsed Time: Manually set the number of days that the air filters have been used.
  3. Tap OK to confirm your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?