990-5452N-001

Start Up and Add UPS to a Running Parallel System

Use this procedure to start up a UPS and add it to a running parallel system.

NOTE: Only operate a disconnect device when the associated disconnect device LED is green.
  1. Close UIB.
    This will power up the display interface after approximately 30 seconds.
  2. From the home screen on the display, select Control > Startup Wizard. Select Startup UPS into a parallel system and follow the steps which appear on the screen.
    NOTE: The following is a generic start-up procedure. Always follow the steps of the Startup Wizard which are specific to your system.
  3. Close SSIB.
  4. Close the backfeed protection switch (BF2) (if present), if it is open.
  5. Close the battery disconnect devices in your specific battery solution.
  6. Close UOB.
  7. Turn the inverter on by tapping the Inverter ON button on the front of the UPS.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?