990-5452N-001

Configure the Display Preferences

  1. From the home screen on the display select Configuration > Display > Preferences.
  2. Select the preferred language using the up and down arrows.
  3. Select the preferred date format using the up and down arrows.
  4. Select the preferred temperature units: US Customary (°Fahrenheit) or Metric (°Celsius).
  5. Set the current date and time using one of the below two methods:
    • Set the date and time manually on the display by selecting Manual and typing the actual date and time and completing with Enter.
    • Set the date and time automatically by selecting Synchronize with NTP server (Network Time Protocol server).
      NOTE: NTP server settings can be configured in the network management interface via the Web, command line, or config file.
  6. Tap OK to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?