990-5452N-001

Configure Automatic Battery Test

  1. From the home screen on the display select Configuration > Battery > Test.
  2. Set your preferred settings for the automatic battery test:
    1. Battery Test Interval: Select your preferred interval for battery tests. Choose between: Never, Every 52 Weeks, Every 26 Weeks, Every 12 Weeks, Every 8 Weeks, Every 4 weeks, Every 2 Weeks, or Once a Week.
      NOTE: If you run battery tests too frequently it can reduce the lifetime of the batteries.
    2. Battery Test Start Time: Select the time of the day in 24 hour format that the test should take place and complete with Enter.
    3. Battery Test Day of the Week: Select the day of the week that the test should take place and complete with Enter.
  3. When all settings have been completed, tap OK to confirm your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?