Configure the Output Relays
- On the display select .
- Select to enable or disable Energized check
mode.
- When Energized check mode is enabled the output relays are ON. If a signal is received or the power supply to the relay is lost, the circuit will open and the relay will be deactivated.
- When Energized check mode is disabled the output relays are OFF. If a signal is received, the circuit will close and the relay will be activated.
- Select the output relay that you wish to configure.
- Select the function that you wish to use the specific output
relay for from the list below:
Common Alarm: The output is triggered when any alarm is present.
Normal Operation: The output is triggered when the UPS is running in normal operation.
Battery Operation*: The output is triggered when the UPS is running in battery operation.
Maintenance Bypass*: The output is triggered when the UPS is running in maintenance bypass operation.
Static Bypass*: The output is triggered when the UPS is running in forced static bypass operation or requested static bypass operation.
High Efficiency Mode: The output is triggered when the UPS is running in eConversion or ECO mode.
Output Overload: The input is triggered when there is an overload condition.
Fan Inoperable: The output is triggered when one or more fans are inoperable.
Battery is not Working Correctly*: The output is triggered when the batteries are not working correctly.
Battery Disconnected*: The output is triggered when the batteries have been disconnected or the battery disconnect device(s) are open.
Battery Voltage Low*: The output is triggered when the battery voltage is below the threshold.
Input Out of Tolerance: The output is triggered when the input is out of tolerance.
Bypass Out of Tolerance*: The output is triggered when the bypass is out of tolerance.
UPS Warning: The output is triggered when a warning alarm is present.
UPS Critical: The output is triggered when a critical alarm is present.
Parallel Redundancy Lost: The output is triggered when the specified redundancy has been lost.
External Fault: The output is triggered when a fault external to the UPS is present.
UPS Maintenance Mode: The output is triggered when the unit output disconnect device (UOB) is open.
System Warning: The output is triggered when a warning alarm is present in a parallel system.
System Critical: The output is triggered when a critical alarm is present in a parallel system.
System Common Alarm: The output is triggered when any alarm is present in a parallel system.
Emergency power off activated: The output is triggered when the EPO has been activated.
Transfer to static bypass disabled
UPS informational alarm: The output is triggered when an information alarm is present.
System informational alarm: The output is triggered when an information alarm is present in a parallel system.
- Set the delay in seconds for the specific output to activate. Select a value between 0 and 60 seconds.
- Tap OK to save your settings.