990-5452N-001

Configure Battery Alarm Threshold

  1. From the home screen on the display select Configuration > Battery > Alarms.
  2. Select your preferred battery alarm threshold in seconds. Select a value between 60 and 6000 seconds and complete with Enter.
  3. Tap OK to confirm your setting.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?