990-5452N-001

Access Password-Protected Screens

  1. When prompted for the password, select your username.
  2. Type in the pin code for your username.
    NOTE: The default pin code is 1234.
  3. Change the password.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?