Important Safety Instructions — SAVE THESE INSTRUCTIONS
Read these instructions carefully and look at the equipment to become familiar with it before trying to install, operate, service or maintain it. The following safety messages may appear throughout this manual or on the equipment to warn of potential hazards or to call attention to information that clarifies or simplifies a procedure.
DANGER |
|---|
|
DANGER indicates a hazardous situation which, if
not avoided, will result in death or serious injury.
Failure to follow these instructions will result in death or serious injury.
|
WARNING |
|---|
|
WARNING indicates a hazardous situation which,
if not avoided, could result in death or serious injury.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
CAUTION |
|---|
|
CAUTION indicates a hazardous situation which,
if not avoided, could result in minor or moderate injury.
Failure to follow these instructions can result in injury or equipment damage.
|
| NOTICE |
|---|
|
NOTICE is used to address practices not related
to physical injury. The safety alert symbol shall not be used with
this type of safety message.
Failure to follow these instructions can result in equipment damage.
|
Please Note
Electrical equipment should only be installed, operated, serviced, and maintained by qualified personnel. No responsibility is assumed by Schneider Electric for any consequences arising out of the use of this material.
A qualified person is one who has skills and knowledge related to the construction, installation, and operation of electrical equipment and has received safety training to recognize and avoid the hazards involved.
Per IEC 62040-1: "Uninterruptible power systems (UPS) -- Part 1: Safety Requirements," this equipment, including battery access, must be inspected, installed and maintained by a skilled person.
The skilled person is a person with relevant education and experience to enable him or her to perceive risks and to avoid hazards which the equipment can create (reference IEC 62040-1, section 3.102).
FCC Statement
UPSs with 1250 kW I/O Cabinet
Any changes or modifications not expressly approved by the party responsible for compliance could void the user’s authority to operate the equipment.
UPSs with 1500 kW I/O Cabinet
Any changes or modifications not expressly approved by the party responsible for compliance could void the user’s authority to operate the equipment.
Electromagnetic Compatibility
UPSs with 1250 kW I/O Cabinet
| NOTICE |
|---|
|
Risk of electromagnetic disturbance
This is a product category C2 UPS product. In a residential
environment, this product may cause radio inference, in which case
the user may be required to take additional measures.
Failure to follow these instructions can result in equipment damage.
|
UPSs with 1500 kW I/O Cabinet
| NOTICE |
|---|
|
Risk of electromagnetic disturbance
This is a product Category C3 according to IEC 62040-2.
This is a product for commercial and industrial applications in the
second environment - installation restrictions or additional measures
may be needed to prevent disturbances. The second environment includes
all commercial, light industry, and industrial locations other than
residential, commercial, and light industrial premises directly connected
without intermediate transformer to a public low-voltage mains supply.
The installation and cabling must follow the electromagnetic compatibility
rules, e.g.:
Failure to follow these instructions can result in equipment damage.
|
Safety Precautions
DANGER |
|---|
|
hazard of electrical shock, explosion or arc flash
All safety instructions in this document must be read,
understood and followed.
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
hazard of electrical shock, explosion or arc flash
After the UPS system has been electrically wired, do not
start up the system. Start-up must only be performed by Schneider
Electric.
Failure to follow these instructions will result in death or serious injury.
|
Electrical Safety
This manual contains important safety instructions that should be followed during the installation and maintenance of the UPS system.
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
The label below must be added if:
-
The UPS input is connected through external isolators that, when opened, isolate the neutral, OR
-
The UPS input is connected via an IT power system.
The label below must be also added if backfeed protection is provided external to the equipment. See Backfeed Protection for more details. The label must be placed adjacent to all upstream power disconnection devices.
DANGER |
|---|
|
Hazard of electric shock, explosion, or arc flash
Risk of voltage backfeed. Before working on this circuit:
Isolate the UPS and check for hazardous voltage between all terminals
including the protective earth.
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
Hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
Add the label below on the UPS if autostart has been enabled:
DANGER |
|---|
|
Hazard of electric shock, explosion, or arc flash
Autostart is enabled. The UPS will automatically restart
when the mains supply returns.
Failure to follow these instructions will result in death or serious injury.
|
| NOTICE |
|---|
|
Risk of unintentional device operation
If a residual current-operated protective device (RCD-B)
is used upstream as ground fault protection, then the RCD-B shall
be sized to not trip on the leakage current of this product. The start-up
leakage current can be up to 3 A. The continuous maximum leakage current
is 350 mA.
Failure to follow these instructions can result in equipment damage.
|
Battery Safety
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
Hazard of electric shock, explosion, or arc flash
Batteries can present a risk of electric shock and high
short-circuit current. The following precautions must be observed
when working on batteries
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
Hazard of electric shock, explosion, or arc flash
When replacing batteries, always replace with the same
type and number of batteries or battery packs.
Failure to follow these instructions will result in death or serious injury.
|
CAUTION |
|---|
|
risk of equipment damage
Failure to follow these instructions can result in injury or equipment damage.
|
DANGER
WARNING
CAUTION
DANGER