990-5452N-001

Configure the Input Contacts

  1. On the display select Configuration > Input Contacts and select the input contact that you wish to configure.
  2. Choose between the below options:

    Custom Input 1: General purpose input.

    External Battery Monitoring Detected Fault: Input to indicate that the external battery monitor has detected a fault.

    Custom Input 2: General purpose input.

    Battery Room Ventilation Inoperable: Input to indicate that the battery room ventilation is inoperable. When the input is active, the battery charger will turn off.

    Ground fault: Input to indicate that a ground fault is present.

    Supplied By Genset: Input to indicate that the UPS is running on generator. The battery charge current will be reduced to the value set by Schneider Electric during start-up.

    Inhibit Transfer from Static Bypass: When this input is active, and the system enters requested static bypass or forced static bypass, the system will be locked in static bypass as long as the input is active.

    External energy storage: minor alarm: Input to indicate that the external energy storage monitor reports a minor alarm.

    External energy storage: major alarm: Input to indicate that the external energy storage monitor reports a major alarm.

    Force the Charger to Turn Off: Input that forces the charger to turn off.

    Flywheel inoperable: Input to indicate that the flywheel is inoperable.

    Disable High Efficiency Mode: Input to disable the use of high efficiency mode

    Request bypass operation: Input that will transfer the UPS into requested static bypass operation if the conditions for a transfer are met.

    Force battery operation: Input that will force a transfer to battery operation.

    Distributed Energy Reserve: Input that will activate Distributed Energy Reserve mode. DC ground fault present: Input that will activate the alarms for DC ground fault.
    Command the UPS to inhibit bypass transfer: Input that will inhibit the UPS from transferring to bypass operation.  
  3. Tap OK to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?