990-5452N-001

Delete a User

  1. From the home screen on the display select Configuration > Display > Security > Delete User.
  2. Browse to the user that you wish to delete using the up and down arrows and tap OK.
  3. Tap Yes to confirm deletion of an existing user of the system.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?