990-5452N-001

Start a Boost Charge of the Batteries

Boost charge gives the possibility of doing a fast recharge of a discharged battery.

NOTE: Boost charge must be enabled by Schneider Electric during start-up for this option to be available.
  1. From the home screen on the display select Control > Charger Mode.
  2. Select Boost Charge to initiate a single boost charge of the batteries.

    The UPS system starts boost charging the batteries.

    To stop the boost charge and go back to float charge, select Float Charge.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?