0602IB1801EN-09

General

Device Physical Location

Step

Action

Result

1

From the IFE menu bar, click Configuration & Settings .

Opens the Configuration & Settings menu.

2

From the Configuration & Settings menu, in the General submenu, click Device Physical Location .

Opens the Device Physical Location page.

3

In Device Physical Location webpage, click Blink ON .

Sets the IFE interface in test mode and the LED blinks in ULP pattern with 1 second ON and 1 second OFF.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?