Devices
Description
The page gives the information about the devices which are connected to the ULP port of the IFE interface. The devices connected are:
-
BCM ULP module
-
MicroLogic control unit
-
BSCM module
-
FDM121 display
-
IO module IO 1
-
IO module IO 2
-
Universal Test Adopter (UTA) module
The users with Installer or Engineer roles can consult the Diagnostics pages.
Navigation to the Devices Page
To view the page, click
Circuit Breakers Parameters
|
Parameter |
Description |
|---|---|
|
|
Displays the rated current of the circuit breaker. |
|
|
Displays the protection type of the circuit breaker. |
|
|
Displays the number of IO modules connected to the circuit breaker. |
|
|
Displays the remaining service life of circuit breaker. |
|
|
Displays the contact wear counters of the circuit breaker. |
|
|
Displays the indication of contact operation of circuit breaker since last reset. |
|
|
Displays the indication of fault trip contact operation of circuit breaker. |
|
|
Displays the status of cradle in connected position. |
|
|
Displays the status of cradle in disconnected position. |
|
|
Displays the status of cradle in test position. |
Components Parameters
|
Device |
Parameter |
Description |
|---|---|---|
|
Circuit Breaker |
|
Name of the device type. |
|
|
Device model number. |
|
|
|
Device serial number. |
|
|
|
Device commercial reference number. |
|
|
|
Current firmware version. |
|
|
IO Module |
|
Device serial number. |
|
|
Device commercial reference number. |
|
|
|
Current firmware version. |