Status
Description
The page displays the IFE interface communication status.
While browsing the real-time data views, the IFE interface has an automated communication check that runs every 15 minutes by default. This check verifies the communication health of all the devices configured on the IFE interface, and attempts to re-establish the communication to any device marked out of service within the current browser session.
A manual communication check is possible by clicking .
The users with Installer or Engineer roles can consult the Diagnostics pages.
Navigation to the Status Page
To view the page, click .
Status Parameters
|
Data |
Description |
|---|---|
|
|
Name of the device connected to IFE interface. |
|
|
Type of the device connected to IFE interface. |
|
|
Displays the connection type: Type 1: ULP |
|
|
Status of communication:
|