Modbus
Description
The page displays the global statistics of TCP/IP and TCP port connections.
The users with Installer or Engineer roles can consult the Diagnostics pages.
Navigation to the Modbus Page
To view the page, click .
Global Statistics Parameters
|
Global Statistics |
Parameter |
Description |
|---|---|---|
|
|
|
Number of frames received |
|
|
Number of frames transmitted |
|
|
|
Status of the connected Ethernet port: If is disabled, the Port Status value is displayed as . |
|
|
|
Number of active connections |
|
|
|
|
Number of frames received |
|
|
Number of frames transmitted |
|
|
|
Number of error messages |
|
|
Click to reset the statistics values to 0. If the IFE interface is switched off or if it is reset due to a configuration change or another event, the statistics values are reset to 0. |
||
Modbus TCP Port Connections Parameters
|
Parameter |
Description |
|---|---|
|
|
Serial number |
|
|
Remote IP address |
|
|
Remote port number |
|
|
Local port number |
|
|
Number of messages transmitted |
|
|
Number of messages received |
|
|
Number of error messages sent |