Device Control
Reset Commands
The page allows you to execute one or more reset commands per device type.
From the menu, in the submenu, on the device list, select the device and click . Select an in the list to reset.
Application Control
The page allows you to control the following applications remotely:
-
Breaker application
-
IO application
By default, this feature is disabled in IFE interface.
Password Management
When the application control operation is performed, an dialog box appears in the IFE webpage. Enter the password in the dialog box to perform the application control operation.
The password required is for PowerPacT H-, J-, and L-frame circuit breaker with BSCM and MasterPacT NT/NW or PowerPact P- and R-frame circuit breaker with BCM ULP.
The following operations in the page require a password:
|
Control |
Operation |
Availability |
|---|---|---|
|
Breaker/Switch disconnector (BCM-OF/SD) |
Open/Close/Reset |
PowerPacT H-, J-, and L-frame circuit breaker with BSCM |
|
Open/Close |
MasterPacT NT/NW or PowerPact P- and R-frame circuit breaker with BCM ULP |
|
|
Light |
On/Off |
IO 1 or IO 2 |
|
Load |
On/Off |
IO 1 or IO 2 |
|
Reset input counters |
I1 I2 I3 I4 I5 I6 |
IO 1 |
|
#I1 #I2 #I3 #I4 #I5 #I6 |
IO 2 |
|
|
Reset output counters |
O1 O2 O3 |
IO 1 |
|
#O1 #O2 #O3 |
IO 2 |
|
|
User-defined output control |
On/Off |
IO 1 or IO 2 |
Enable Application Control in IFE Interface
Follow the below procedure to enable the feature in IFE interface.
|
Step |
Action |
Result |
|---|---|---|
|
1 |
Press the test button on the front face of the IFE interface for 10–15 s. NOTE: Do not press
the test button less than 10 s or more than 15 s.
|
Initiates the application control feature. |
|
2 |
After 15 s, IFE interface initiates the application control feature. |
The feature disclaimer window is available continuously for 5 min. The module status LED starts blinking continuously for 5 min (1 s ON, 1 s OFF) once the test button is released. |
|
3 |
Access the IFE webpage and login as an administrator. |
The administrator logs in to the IFE webpage. |
|
4 |
From the menu, click . |
The reads the disclaimer and chooses either the option or . The application control feature disclaimer is: By accepting this disclaimer, you are directed to webpage access which enables you to control several applications remotely. It is highly recommended that the administrator modify the default administrator password. By using, you are agreeing to indemnify and hold harmless Schneider Electric for and from any claims, losses, demands, lawsuits, and damages that are a result of direct or indirect use of this application control feature by reason of any act or emission which the user commits. The disclaimer page is available in the language selected by the administrator. |
|
5 |
Select . |
The application control feature is now enabled for the administrator. The breaker application and IO application are enabled in the webpage access for providing access to the other user groups. |
|
6 |
Select . |
The application control feature is disabled. The breaker application and IO application are disabled in the webpage access. |
Breaker Application
From the page, in the , the authorized group can perform the following operations:
|
Control |
Status |
Operation |
Availability |
|---|---|---|---|
|
Breaker |
Open/Close/Tripped/NA |
Open/Close/Rest |
PowerPacT H-, J-, and L-frame circuit breaker with BSCM |
|
Open/Close |
MasterPacT NT/NW or PowerPact P- and R frame circuit breaker or switch disconnector with BCM ULP |
IO Application
From the page, in the , the authorized group can perform the following operations:
|
Control |
Status |
Operation |
Availability |
|---|---|---|---|
|
Reset input counters |
– |
I1 I2 I3 I4 I5 I6 |
IO 1 |
|
#I1 #I2 #I3 #I4 #I5 #I6 |
IO 2 |
||
|
Reset output counters |
– |
O1, O2, O3 |
IO 1 |
|
#O1 #O2 #O3 |
IO 2 |
||
|
Light control |
ON or OFF |
ON / OFF |
IO 1 or IO 2 |
|
Load control |
ON or OFF |
ON / OFF |
IO 1 or IO 2 |
|
User-defined output control |
ON or OFF |
ON / OFF |
IO 1 or IO 2 |
-
The IO application control is possible only when the IO module is connected to a circuit breaker.
-
The light and the load control are available when the application rotary switch of IO 1 or IO 2 is in position 4.
-
The user-defined output control is available only when the user-defined output has been assigned with EcoStruxure Power Commission software.
-
If the input is assigned as a pulse counter, the operation is P1, P2, P3, P4, P5, and P6 for IO 1. For IO 2, the pulse counter operation is #P1, #P2, #P3, #P4, #P5, and #P6.