Date and Time
Description
The page allows you:
-
To manually set the date and time of the circuit breaker connected to the IFE interface
. -
To automatically synchronize the date and time of the circuit breaker to the IFE time
-
To periodically check the synchronization at specified interval of time
List of Parameters in Date and Time Configuration
|
Parameter |
Description |
|---|---|
|
|
Allows you to select the manual date and time setting of the circuit breaker connected to the IFE interface. This option is disabled when is selected. |
|
|
Allows you to set the present date manually in the format YYYY-MM-DD. |
|
|
Allows you to set the present time manually in the format hh:mm:ss. |
|
|
Allows you to enable the automatic time setting of the circuit breaker connected to the IFE interface. This option is disabled when is selected. |
|
|
Allows you to enter the poll interval in hours that ranges from 1 through 63. |
|
|
Allows you to enable the check box that obtains the server address from DHCP or BOOTP. |
|
|
Allows you to enter the primary SNTP server address. |
|
|
Allows you to enter the secondary SNTP server address. |
|
|
Allows you to automatically synchronize the time of the circuit breaker connected to the IFE interface with the IFE time. |
|
|
Allows you to clear the synchronization of the circuit breaker connected to the IFE interface. |
Setting the IFE Date and Time Manually
|
Step |
Action |
Result |
|---|---|---|
|
1 |
From the IFE menu bar, click . |
Opens the menu. |
|
2 |
In the submenu, click and then select from the . |
The parameters for date and time settings is available. |
|
3 |
Enter the date in the format YYYY-MM-DD. |
Sets the date of the IFE interface manually. |
|
4 |
Enter the time in the format hh:mm:ss. |
Sets the time of the IFE interface manually. |
|
5 |
Click . |
The date and time of IFE interface is set. |
Setting the IFE Date and Time Automatically with SNTP
|
Step |
Action |
Result |
|---|---|---|
|
1 |
From the IFE menu bar, click . |
Opens the menu. |
|
2 |
In the submenu, click and then select from the . |
The circuit breaker connected to the IFE interface is selected by default for date and time synchronization. |
|
3 |
Enter the poll time in the box. |
The entered time is updated. |
|
4 |
Select to obtain SNTP server automatically via DHCP/BOOTP. |
The SNTP server address is obtained automatically. |
|
5 |
Enter the primary and secondary server address in the and box. |
The entered SNTP server address is updated. |
|
8 |
Click . |
The date and time of the circuit breaker get synchronized with the IFE time. |