Real Time Data
Description
The page provides:
-
The basic readings of the circuit breaker connected to the IFE interface in real time on .
-
The circuit breaker summaries on .
-
The real-time trending for the circuit breaker for the selected topics on .
Single Device Pages
This page displays the basic readings of the circuit breaker connected to the IFE interface on real-time basis. This includes circuit breaker health status with green, orange, and red indication, cradle status, load current, power, power factor, voltage, and so on.
The table shows the steps to monitor the real-time data of a device:
|
Step |
Action |
Result |
|---|---|---|
|
1 |
From the IFE menu bar, click . |
Opens the menu. |
|
2 |
From the menu, in the submenu, select the circuit breaker from . |
Displays the real-time data of the circuit breaker. |
Summary Device Pages
The summary device table views provide summary of the circuit breaker connected to the IFE interface.
|
Step |
Action |
Result |
|---|---|---|
|
1 |
From the menu, in the submenu, click . |
Expands the tree for summary page selection choices. |
|
2 |
Select the to be viewed. |
Opens the device selection list. |
|
3 |
Select the circuit breaker from the , then click . NOTE: Click to select all the available devices. Click to clear all the selected
devices.
|
Summary of the circuit breaker appears. NOTE: Click to navigate back to the device selection list.
|
Trending
|
Step |
Action |
Result |
|---|---|---|
|
1 |
From the IFE menu bar, click . |
Opens the menu. |
|
2 |
From the menu, in the submenu, select . |
Expands the data tree for real-time data option selection and the time trending option selection. |
|
3 |
Select . |
Opens the real-time trending setup page. |
|
4 |
Select the circuit breaker from the list. |
Selects the circuit breaker for trending. |
|
5 |
Select up to 8 topics from the list. |
Selects topics for trending. |
|
6 |
Click to open the display page. |
Opens the real-time trending display page. |
|
7 |
Set the trending parameters. |
Allows trending parameters to be set. |
Trending Parameters
|
Step |
Action |
Result |
|---|---|---|
|
1 |
Select or trending. NOTE:
redraws the x-axis in the graph
after each sample, filling it with all the data collected since the
start of the trend. The updates the graph with the latest data after each sample
while the x-axis stays constant to show the overall trend time selected.
|
Selects graph mode. |
|
2 |
Choose a trend time from 1–15 minutes. This is the duration of the trend. |
Selects the amount of time of the trend. |
|
3 |
Select to start the trending of the selected topics. NOTE: Trending may be stopped
before reaching the trend time by clicking . If is pressed after stopping
the sampling, a new trend is started.
|
Starts trending. |
|
4 |
Press to view a log of all the sampled topics recorded during the trend time. |
Displays a log of all topic values sampled during the trend. |
|
5 |
Press to reselect the devices and topics to trend. |
Navigates back to the real-time trending setup page. |