Webpage Description
Monitoring Webpage
|
Monitoring Submenu |
Webpage |
Description |
|---|---|---|
|
|
The single device pages provide basic readings of the circuit breaker connected to the IFE interface. |
|
|
The summary device pages provide summaries of the circuit breaker connected to the IFE interface. |
||
|
The trending page view provides real-time graphic and table trending of the circuit breaker connected to the IFE interface. |
||
|
|
The single device pages provide the graphic and table trending logs of user-selectable quantities for circuit breaker connected to the IFE interface. |
|
|
The summary device pages provide graphic trending logs of the circuit breaker connected to the IFE interface. |
Control Webpage
Diagnostics Webpage
|
Diagnostics Submenu |
Webpage |
Description |
|---|---|---|
|
|
Displays diagnostic data used to troubleshoot the network-related problems. |
|
|
|
|
|
|
Displays the list of the IMU devices connected to the ULP port. |
||
|
|
Displays register data connected locally to the IFE interface. |
|
|
Verifies the communication health of the circuit breaker connected to the IFE interface. |
||
|
|
Displays the status of IO module connected to the circuit breaker. Displays if the circuit breaker is not connected to a IO module. NOTE:
refers to the circuit
breaker name defined in the page.
|
Maintenance Webpage
Configuration & Settings Webpage
|
Configuration & Settings Submenu |
Webpage |
Description |
|---|---|---|
|
|
|
|
|
Sets the date and time manually or sets the IFE time automatically using an SNTP source or configures the device connected to IFE interface to synchronize their time with the IFE time automatically. |
||
|
Configures the time zone for the region and sets the daylight saving time. |
||
|
|
Configures the Ethernet. |
|
|
Configures the IP parameters. |
||
|
Configures the maximum number of Modbus TCP/IP server connections. Configures the IP addresses that can access the IFE interface through Modbus TCP/IP. |
||
|
|
Configures the alarms to be emailed. Configures the SMTP parameter for mailing purpose. |
|
|
Configures the alarms to be sent through email. |
||
|
|
Configures the circuit breaker connected to the IFE interface. |
|
|
Configures device logging parameters. |
||
|
Configures device logging export options. |
||
|
|
Configures Simple Network Management Protocol (SNMP). |
|
|
Configures IFE preferences. |
||
|
Configures the advanced service control parameters. |
||
|
Creates and edits groups and users. Configures email accounts. |
||
|
Configures webpage access rights for each user group. |