Set Device Time
Description
The page allows you to synchronize the date and time of the circuit breaker connected to the IFE interface to IFE date and time.The time is set automatically. This page is used to get the circuit breaker time.
List of Parameters in Set Device Time
|
Parameter |
Description |
|---|---|
|
|
Allows you to select the circuit breaker that is to be synchronized with IFE date and time. |
|
|
Displays the time of the circuit breaker. |
|
|
Displays the status of the circuit breaker. |
|
|
Allows you to get the time of the circuit breaker. |
|
|
Not applicable. |
Setting the Device Time
|
Step |
Action |
Table |
|---|---|---|
|
1 |
From the IFE menu bar, click . |
Opens the menu. |
|
2 |
From the menu, click . |
Opens the page. |
|
3 |
Select the circuit breaker from the page and then click . |
The date and time of the circuit breaker gets synchronized with the IFE date and time, and the status is updated as successful. NOTE: If the circuit breaker fails to synchronize with
IFE
date and time, then the status is updated as unsuccessful.
|