Devices
Description
The page allows you to select the data of the device connected to the IFE interface to publish (24 data maximum).The way to publish the data is set on the page Data Publishing.
The device connected to the IFE interface ULP port is automatically detected and added to the IFE interface in the device list.
The users with Installer or Engineer role can change the device settings.
Navigation to the Devices Page
To view the page, click .
Device Settings
|
Setting |
Description |
Value |
|---|---|---|
|
|
Displays the device type. NOTE: The field is auto-detected and it is unavailable to edit.
|
– |
|
|
Allows you to enter the names of the devices. NOTE:
|
The device name can have up to 64 ASCII characters with the following characters: A–Z, a–z, 0–9, and -. However, - cannot be used at the beginning or at the end of the name. NOTE:
|
|
|
Displays the device IP address and the local address of the device connected to the IFE interface or remote device.
|
For port: 255 (Default setting) |
|
|
Allows you to enable the publication of data from the device connected to the IFE interface (disabled by default). The data is selected to publish while is enabled. |
There are eight categories for data publishing Default values: Apparent Energy (kVAh) Active Energy (kWh) Reactive Energy (kVARh) |
Selection of the Data to Publish
The data to publish are listed in 8 categories:
In each category, the list of data to publish is adapted to the device connected to the IFE interface.
A maximum of 24 data can be selected for publication, out of which the following 3 data are selected by default: