Schematics with MasterPacT NT/NW and PowerPacT P- and R-Frame Circuit Breakers
Description
Depending on the type of circuit breaker used, connect the IFE interface to the circuit breaker using one of the following configurations:
-
Connection of the IFE interface to a fixed manually-operated PowerPacT P- and R-Frame circuit breaker with a BCM ULP module.
-
Connection of the IFE interface to a fixed electrically-operated MasterPacT NT/NW or PowerPacT P-frame circuit breaker with a BCM ULP module.
-
Connection of the IFE interface to a drawout MasterPacT NT/NW or PowerPacT P-frame circuit breaker with a BCM ULP module and its respective IO module.
For more information, refer to the ULP System User Guide.
ULP Connection
| NOTICE |
|---|
|
HAZARD OF EQUIPMENT DAMAGE
Failure to follow these instructions can result in equipment damage.
|
All connection configurations require the BCM ULP cord.
When the second RJ45 ULP port is not used, it must be closed with a ULP line termination.
|
A |
Circuit breaker BCM ULP cord or RJ45 plug/plug ULP cord |
|
B |
ULP line termination |
Connection of the IFE Interface to a Fixed Manually-Operated PowerPacT P- and R-Frame Circuit Breaker
|
A |
IFE Ethernet interface for one circuit breaker |
|
B |
ULP line termination |
|
C |
Circuit breaker BCM ULP cord |
|
D |
BCM ULP circuit breaker communication module |
|
E |
Fixed manually-operated PowerPacT P- and R-Frame circuit breaker |
Connection of the IFE Interface to a Fixed Electrically-Operated MasterPacT NT/NW or PowerPacT P-Frame Circuit Breaker
|
A |
IFE Ethernet interface for one circuit breaker |
|
B |
ULP line termination |
|
C |
Circuit breaker BCM ULP cord |
|
D |
Fixed terminal block |
|
E |
BCM ULP circuit breaker communication module |
|
F |
Fixed electrically-operated circuit breaker |
Connection of the IFE Interface to a Drawout MasterPacT NT/NW or PowerPacT P-Frame Circuit Breaker
|
A |
IFE Ethernet interface for one circuit breaker |
|
B |
ULP line termination |
|
C |
RJ45 plug/plug ULP cord |
|
D |
Circuit breaker BCM ULP cord |
|
E |
Circuit breaker disconnected position contact (CD) |
|
F |
Circuit breaker cradle |
|
G |
BCM ULP circuit breaker communication module |
|
H |
Drawout circuit breaker |
|
I |
Drawout terminal block |
|
J |
Circuit breaker connected position contact (CE) |
|
K |
Circuit breaker test position contact (CT) |
|
L |
IO input/output application module for one circuit breaker |