0602IB1801EN-09

Emails

Description

The EMAILS page allows you to set the list of recipients of emails for:

  • Event notification

  • Data publishing

A maximum of 15 users or email recipients can be declared.

The users with Installer or Engineer roles can change the Emails settings.

Navigation to the Emails Page

To view the EMAILS page, click SETTINGS > CONTACT MANAGEMENT > EMAILS .

List of Settings

Setting

Description

Email

Allows you to enter the email address of the recipient.

Language

Displays the name selected language. Email Language Settings

Notification

Allows you to select the events from the list to notify the user through email.

Data Publishing

Allows you to enable publication through email of the data selected on the DEVICES page Devices.

Notification Page

The Notification page allows the selection of the events to notify through email among a list of events.

CAUTION
EQUIPMENT INCOMPATIBILITY OR INOPERABLE EQUIPMENT
Do not rely solely on the notification of the emails for maintaining your equipment.
Failure to follow these instructions can result in injury or equipment damage.

The list of event displayed contains only applicable events related to the devices connected to the ULP port of the IFE interface.

NOTE: If an email SMTP server is not located on the same Ethernet network segment as IFE interface, ensure that the IFE default gateway is properly configured.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?