IP Configuration
IPv4 Configuration
|
Parameter |
Description |
Settings |
|---|---|---|
|
|
Used to select the mode for assigning the IPv4 parameters set. Obtain IPv4 parameters automatically using BOOTP or DHCP. NOTE: While using a legacy DHCP server, the device name must be limited to 16 characters.
|
|
|
|
Used to enter the static IP address of an IFE interface. |
– |
|
|
Used to enter the Ethernet IP subnet mask address of your network. |
– |
|
|
Used to enter the gateway (router) IP address used for wide area network (WAN) communication. |
– |
IPv6 Configuration
|
Parameter |
Description |
Settings |
|---|---|---|
|
|
Defines the IPv6 configuration. |
(Default setting) NOTE: The setting
is unavailable to edit.
|
|
|
Used to open the IFE webpage for future use. NOTE: In the URL address box, use [ ] brackets to enter the
link local address.
|
– |
DNS
|
Parameter |
Description |
Setting |
|---|---|---|
|
|
Defines the dynamic behavior of the DNS server address configuration. Used to obtain the IP address from the DNS server automatically. NOTE: Domain name system (DNS) is the naming system for computers and devices
connected to a local area network (LAN) or the Internet.
|
Disabled when manual setting is selected. |
|
|
Defines the IPv4 address of the primary DNS server. |
– |
|
|
Defines the IPv4 address of the secondary DNS server. Used to perform a DNS resolution when the resolution fails with the primary DNS server. |
– |
Duplicate IP Address Detection
While connected to your network, the IFE interface publishes its IP address. To avoid any duplicate IP address conflicts, the IFE interface uses the address resolution protocol (ARP) to see if any other device on your network is using the same IP address. The following table explains how the IFE interface handles a duplicate IP address when it is detected.
Duplicate IP Address Scenario
|
Scenario |
Duplicate IP Detected |
Network Status LED |
|---|---|---|
|
Ethernet link detected |
Reverts to the default IP address, subnet mask, and gateway address. ARP requests are sent every 15 seconds until the IP address is available. IFE interface uses the IP address when it is available, |
Steady red |
|
Manual address change |
Reverts to the default IP address, subnet mask, and gateway address. The ARP requests are sent every 15 seconds until the IP address is available. The IFE interface uses the IP address when it is available. |
Steady red |
|
Receives an ARP request |
If more than one ARP is detected within 10 seconds, initiate the process to reacquire the IP. |
OFF |