Ethernet Configuration (Dual Port)
Ethernet
|
Parameter |
Description |
Settings |
|---|---|---|
|
|
A unique media access control address of an IFE interface. The MAC address is written on the label which is placed on the side of the IFE interface. |
– |
|
|
Used to select the format for data sent over an Ethernet connection. NOTE: Whenever the frame format settings are changed, restart
the device to implement the changes.
|
|
Ethernet Port Control
|
Parameter |
Description |
Settings |
|---|---|---|
|
|
Used to define the physical Ethernet connection speed and transmission mode for Ethernet port 1. |
(Default setting) |
|
|
Used to define the physical Ethernet connection speed and transmission for Ethernet port 2. |
(Default setting) |
Broadcast Storm Protection
|
Parameter |
Description |
Settings |
|---|---|---|
|
|
Defines the storm protection level. The level value corresponds to a committed information rate (CIR) value, that is, the amount of traffic entering the switch port from which the storm protection drops entering the broadcast traffic. NOTE: If the level value is changed, you are prompted
to restart the device to implement changes.
|
Broadcast storm protection level:
NOTE: The level value corresponds to the committed information
rate.
|
|
|
Defines the read-only value of broadcast the storm protection level. |
– |