Preferences
Description
The page allows you to set the IFE interface preferences for data refreshment rate.
The users with Installer or Engineer roles can change the preferences settings.
Navigation to the Preferences Page
To view the page, click .
Preferences Settings
|
Parameter |
Description |
Value |
|---|---|---|
|
|
Sets how often data is read from the device in the standard monitoring table views. |
Setting range: 5–60 s Default setting: 5 s |
|
|
Sets how often a communications check is performed while the browser is displaying real-time readings in the standard monitoring table views. This function attempts to bring any out-of-service devices back into service automatically. |
Setting range: 5–30 min Default setting: 15 min |