IFE
Description
The IFE page displays the information of the IFE interface connected to the circuit breakers.
The users with Installer or Engineer roles can consult the Diagnostics pages.
Navigation to the IFE Page
To view the IFE page, click .
IFE Interface Parameters
|
Parameter |
Description |
|---|---|
|
|
Device serial number |
|
|
Device commercial reference number |
|
|
Current firmware version |
|
|
Combination of MAC address and the time |
|
|
Unique MAC address |
|
|
IPv4 address of the IFE interface |
|
|
IPv6 address used to communicate on the local network |
Date and Time Parameters
|
Parameter |
Description |
|---|---|
|
|
Source of time with which the last synchronization has happened |
|
|
Elapsed time from last synchronization |
|
|
Status of NTP Synchronization |
|
|
Describes the accuracy of NTP time. It can take values from 1 to 15 or as NA (not applicable) if NTP server is not reachable. |
File System Parameters
|
Parameter |
Description |
|---|---|
|
|
Total amount of the IFE interface disk size in kilobytes |
|
|
Total amount of used disk size on the IFE interface disk in kilobytes |
|
|
Total amount of unused disk space on the IFE interface disk in kilobytes |
|
|
Amount of corrupted disk space on the IFE interface disk in kilobytes |
System Parameters
|
Parameter |
Description |
|---|---|
|
|
Status of the CPU:
|
|
|
Status of the boot memory |
|
|
Status of EEPROM |
|
|
Status of the file system |
|
|
Status of PHY 1 hardware |
|
|
Status of PHY 2 hardware |
|
|
Status of the execution memory |
IFE Operating Time Parameters
|
Statistic |
Description |
|---|---|
|
|
Operating time of IFE interface |