Ethernet
Description
The page allows you to define the physical Ethernet connection speed and transmission rate for the Ethernet ports.
The users with Installer or Engineer roles can change the Ethernet settings.
For Ethernet settings, after clicking , a pop-up message is displayed for confirmation to restart the interface to apply the new settings:
-
Click to restart and apply the setting changes.
-
Click to cancel the setting modifications and return to the last saved settings.
Navigation to the Ethernet Page
To view the page, click .
Ethernet Settings
|
Parameter |
Description |
Value |
|---|---|---|
|
|
A unique media access control address of an IFE interface. The MAC address is written on the label which is placed on the side of the IFE interface. |
– |
|
|
Used to select the format for data sent over an Ethernet connection. |
|
Port Control Settings
|
Parameter |
Description |
Value |
|---|---|---|
|
|
Used to define the physical Ethernet connection speed and transmission mode for Ethernet port 1. |
Auto-negotiation (default setting) |
|
|
Used to define the physical Ethernet connection speed and transmission for Ethernet port 2. |
Auto-negotiation (default setting) |
Broadcast Storm Protection Settings
|
Parameter |
Description |
Value |
|---|---|---|
|
|
Enables the Broadcast Storm Protection (enabled by default). |
– |
|
|
Allows you to select the broadcast storm protection level. The level value corresponds to a committed information rate (CIR) value, that is, the amount of traffic entering the switch port from which the storm protection drops entering the broadcast traffic. |
Broadcast storm protection level:
NOTE: The level value corresponds to the committed information
rate.
|
|
|
Displays the read-only value of the broadcast storm protection level. |
– |