IP Configuration
Description
The page allows you to set the IP parameters.
The users with Installer or Engineer roles can change the IP configuration settings.
Navigation to the IP Configuration Page
To view the page, click .
IPv4 Settings
|
Parameter |
Description |
|---|---|
|
|
Allows you to select the IPv4 configuration mode:
|
|
|
Allows you to select the mode for assigning the IPv4 parameters by using:
NOTE: While using a legacy DHCP server, the device name must be limited to 16 characters.
|
|
|
Used to enter manually the static IP address of an IFE interface. |
|
|
Used to enter manually the Ethernet IP subnet mask address of your network. |
|
|
Used to enter manually the gateway (router) IP address used for wide area network (WAN) communication. |
IPv6 Settings
For IPv6 Configuration settings, after clicking , a pop-up message is displayed for confirmation to restart the interface to apply the new settings:
-
Click to restart and apply the setting changes.
-
Click to cancel the setting modifications and return to the last saved settings.
|
Parameter |
Description |
|---|---|
|
|
Enables IPv6 (Default setting: Enable). |
|
|
Static IP address of IFE interface. NOTE: In the URL address box, use [ ] brackets to enter the link local address.
|
DNS Settings
|
Parameter |
Description |
|---|---|
|
|
Allows you to select the IPv4 configuration mode:
NOTE: Domain name system (DNS) is the naming system
for computers and devices connected to a local area network (LAN)
or the Internet.
|
|
|
Used to enter manually the IPv4 address of the primary DNS server. |
|
|
Used to enter manually the IPv4 address of the secondary DNS server. Used to perform a DNS resolution when the resolution fails with the primary DNS server. |
Duplicate IP Address Detection
While connected to your network, the IFE interface publishes its IP address. To avoid any duplicate IP address conflicts, the IFE interface uses the address resolution protocol (ARP) to see if any other device on your network is using the same IP address. The following table explains how the IFE interface handles a duplicate IP address when it is detected.
Duplicate IP Address Scenario
|
Scenario |
Duplicate IP Detected |
Network Status LED |
|---|---|---|
|
Ethernet link detected |
Reverts to the default IP address, subnet mask, and gateway address. ARP requests are sent every 15 seconds until the IP address is available. IFE interface uses the IP address when it is available, |
Steady red |
|
Manual address change |
Reverts to the default IP address, subnet mask, and gateway address. The ARP requests are sent every 15 seconds until the IP address is available. The IFE interface uses the IP address when it is available. |
Steady red |
|
Receives an ARP request |
If more than one ARP is detected within 10 seconds, initiate the process to reacquire the IP. |
OFF |