Statistics
Description
The page shows the readings accumulated since the IFE interface was last activated. If the power to the IFE interface is terminated or the device is reset due to a configuration change or other event, all cumulative values are reset to 0.
Reset Procedure
|
Step |
Action |
Result |
|---|---|---|
|
1 |
From the IFE menu bar, click . |
Opens the menu. |
|
2 |
From the menu, in the submenu, click . |
Opens the page. |
|
3 |
View the data. |
See the statistics for each group. |
|
4 |
Click . |
Resets the IFE cumulative diagnostic data to 0. |
Interpreting Ethernet Statistics
|
Global Statistic |
Description |
|---|---|
|
|
Number of frames received |
|
|
Number of frames transmitted |
|
|
Resets the transmitted and received frames |
|
Statistic Per Port |
Description |
|---|---|
|
|
Operational speed (10 Mbps or 100 Mbit/s) |
|
|
Current mode of operation (full duplex or half duplex) |
Interpreting Modbus TCP/IP Statistics
|
Statistic |
Description |
|---|---|
|
|
Status of the connected Ethernet port |
|
|
Number of active connections |
|
|
Number of messages received |
|
|
Number of messages transmitted |
|
|
Resets the received and transmitted messages |
Interpreting System Statistics
|
Statistic |
Description |
|---|---|
|
|
Status of the CPU:
|
|
|
Healthiness of the boot memory |
|
|
Healthiness of EEPROM |
|
|
Healthiness of the file system |
|
|
Healthiness of PHY 1 hardware |
|
|
Healthiness of PHY 2 hardware |
|
|
Healthiness of the execution memory |
Interpreting Date and Time Statistics
|
Statistic |
Description |
|---|---|
|
|
Current date |
|
|
Current time |
|
|
Run time during the system power-up |
Interpreting Date /Time Synchronization
|
Statistic |
Description |
|---|---|
|
|
|
|
|
Time elapsed since the last synchronization has happened |
|
|
Source of time with which the last synchronization has happened |
|
|
Last synchronization date |
|
|
Last synchronization time |
|
|
|
|
|
The following is the status of synchronization with SNTP:
|
Interpreting Modbus Serial Statistics
|
Statistic |
Description |
|---|---|
|
|
A counter that increments each time a frame is sent. |
|
|
A counter that increments each time a frame is received. |
|
|
An error marked from the device or the response timeout. |
Interpreting ULP Statistics
|
Statistic |
Description |
|---|---|
|
|
Number of CAN frames transmitted successfully |
|
|
Number of CAN frames received successfully |
|
|
Maximum number of CAN transmitted errors (TEC) |
|
|
Maximum number of CAN received errors (REC) |
|
|
CAN Bus off count |
|
|
Maximum number of bus off counts |
Interpreting File System Statistics
|
Statistic |
Description |
|---|---|
|
|
Total amount of the IFE disk size in kilobytes |
|
|
Total amount of used disk size on the IFE disk in kilobytes |
|
|
Total amount of unused disk space on the IFE disk in kilobytes |
|
|
Amount of corrupted disk space on the IFE disk in kilobytes |
Interpreting TCP Port Connections Statistics
|
Statistics |
Description |
|---|---|
|
|
Remote IP address |
|
|
Remote port number |
|
|
Number of messages transmitted |
|
|
Number of messages received |
|
|
Number of error messages sent |
|
|
Resets the transmitted and received messages |